Antofagasta, Chile
SM Cyclo de Chile, Ltda.
Antofagasta
Antofagasta
Chile
Tel: | +56 55 256 1611 |
---|---|
Fax: | +56 55 256 1616 |
Email: | [email protected] |
- Assembly
- Sales Office
SM Cyclo de Chile, Ltda. (SMCH) through its plant in Antofagasta is responsible for supplying the northern area of Chile with HANSEN, SEISA, CYCLO®, PARAMAX® and HSM products. Also, since it is in the mining center of the country, it is a leader in repair and maintenance of power transmission in the area. Without a doubt, the excellence of Sumitomo Drive Technologies in the region is due to our presence in this central part of the Andean Region.
Key Facts
Opening
August 8, 2009
Total Area
600 m²
Location
La Negra, Antofagasta